AnsweredAssumed Answered

Low Power MOSFET/PA models for UWB

Question asked by khseah on Apr 27, 2009
Dear All,

I am currently working on Ultra Wideband standard, which spans from 3-10 GHz range, and has a bandwidth of 528 MHz.

I need an appropriate low-power amplifier/MOSFET model that is able to fulfill the bandwidth requirement anywhere in the frequency range. Furthermore, it needs to cater to the low power, preferably with input P1db compression point below -10 dBm.

Can anyone advise me on this?

Thanks
KH  

Outcomes