AnsweredAssumed Answered

Via2 layout component definition

Question asked by aadetoro on Mar 30, 2009
Latest reply on May 7, 2009 by ALEPEREZ
I have defined a substrate in momentum as follows:

---strip - layer_1
alumina (via hole)
---strip - layer_2
alumina_1 (via hole)
strip - layer_3
alumina_2
///GND///

i placed the library component VIA2 on the layout.  I defined it with:
Cond1Layer = "layer_1"
Cond2Layer = "layer_3"

My question has to do with the Height parameter, it is by default = 25.00 mils.  Will my substrate definition override this height parameter as to the actual length of the via?  

Outcomes