AnsweredAssumed Answered

Instrument Options/Control on b1505a

Question asked by andrews on Apr 14, 2016
Latest reply on Apr 14, 2016 by ELSES

I am having problems running a capacitance measurement through IC CAP.  Whenever I run the same measurement on just the 1505, everything works great.  When I try to run the same measurement through IC CAP I am getting bad values (negative capacitances, and noise).  I suspect it has something to do with the instrument options.  Is there a way to import the instrument options/settings from an application test on the 1505, and use them in IC CAP?

Outcomes