I have a circuit that I try to model using the Advanced Model Composer (AMC). After some 350 instances I get the message that the adaptive procedure in selecting parameter values failed and that a constant step will be used instead. AMC then starts over and comes to a solution after 50 instances. My question is, will the final model be based on the last 50 instances only, or all 400?
When non-convergence during modeling process occurs, AMC will default to a preset grid, and only samples on this grid are used.