AnsweredAssumed Answered

Edge Mesh in Momentum

Question asked by HANKE on Feb 6, 2007
Latest reply on Feb 6, 2007 by ALEPEREZ
Hello,
I´m simulating integrated coils with Momentum in ADS 2005a. The coil windings are located in the upper metallization layers, where I want to have the egde mesh opotion for highest accuracy. The rather complicated filling metal layers below act only as capacitive coupling structures to the substrate. Eddy currents can be neglected due to the small size of the metal features. There I don´t want to use edge mesh for saving computation time. If I deselect global edge mesh and activate this option only for selected winding metal layers the edge mesh is not generated after mesh precomputation.
Is there a work around?

Regards

Christian Hanke  

Outcomes