AnsweredAssumed Answered

digital sub-circuits in analog circuit. OFDM

Question asked by D.BUDIMIR on Apr 25, 2007
Latest reply on Apr 25, 2007 by wrivas
Hello,

I have an analog circuit (Envelope simulation) and want to test it with OFDM signal. In ADS analog signal sources there are no OFDM source, but there are some in digital circuits.

Is it possible to use the source from digital circuit in analog one?

Which simulation controllers are suitable for this (in analog circuit I am using Envelope and which one should be used in digital circuit)?

Or may be it is simpler to create OFDM signal source in my analog circuit?

Thank you for your attention.
Best regards!  

Outcomes