Hello everybody,
I´ve got the following problem:
I am designing multi-stage power amplifiers for UMTS (2.14GHz) and therefore I´m using em-cosimulation for characterization of the interconnects and matching networks to get more realistic simulation results. As the flanges of my final stage transistor are ~15mm wide I need pads with a width of about 18mm.
Within my simulation I use 1 port (centered and on the edge of the pad) to connect the drain of the final stage transistor with its pad and output matching network. As I don´t measure the simulated output power (measurement is ~3dB below simulation ) I ask myself if it´s correct to simulate a transistor output with a physical extension of about 15mm with a single port. ???
The simulation results are quite independent of the used mesh density but very sensitive to the positioning of the port. For example, by placing the port a bit more (1...2mm) into the pad I get a variation of output power of about 8dB. :o
So my question is: Has anybody experience with modeling such wide pads or rather injecting energy into a circuit by using a physically extended source? Are there perhaps tricks with the meshing I can do?
Hope someone can help me!
Greetings!!!
Thomas
I´ve got the following problem:
I am designing multi-stage power amplifiers for UMTS (2.14GHz) and therefore I´m using em-cosimulation for characterization of the interconnects and matching networks to get more realistic simulation results. As the flanges of my final stage transistor are ~15mm wide I need pads with a width of about 18mm.
Within my simulation I use 1 port (centered and on the edge of the pad) to connect the drain of the final stage transistor with its pad and output matching network. As I don´t measure the simulated output power (measurement is ~3dB below simulation ) I ask myself if it´s correct to simulate a transistor output with a physical extension of about 15mm with a single port. ???
The simulation results are quite independent of the used mesh density but very sensitive to the positioning of the port. For example, by placing the port a bit more (1...2mm) into the pad I get a variation of output power of about 8dB. :o
So my question is: Has anybody experience with modeling such wide pads or rather injecting energy into a circuit by using a physically extended source? Are there perhaps tricks with the meshing I can do?
Hope someone can help me!
Greetings!!!
Thomas