AnsweredAssumed Answered

State Analyzer Bit Decoder

Question asked by Brig Asay Employee on Oct 15, 2008
This is a working example of a logic state analyzer via UDF. It uses the “Clock Data” function type so you can use the CDR or explicit clock choices in the SDA tool.

It puts the 1’s and 0’s in a text window which you can copy & paste into another file.  

Outcomes