AnsweredAssumed Answered

Problem with a ring 2

Question asked by FRANCISCO on Oct 11, 2005
Latest reply on Oct 13, 2005 by ALEPEREZ
Hello:

I'm sorry, I still have problems with the ring.

What I want to do is to create something similar to the object "MLCLE" from the Library "TLines-Multilayer", but whith other parameters. I have to create 4 rings, one inside the other, so I have 8 parameters, for the 8 radios.

Normaly, I create the rings from circles on different layers, and doing a Boolean Logical. My problem is, after that, how to introduce the 8 radios as parameters.

Thank you very much.  

Outcomes