AnsweredAssumed Answered

Nested DC paramSweep convergence problem

Question asked by FRADEP_eesof on Aug 2, 2005
Latest reply on Aug 3, 2005 by FRADEP_eesof
I noticed a problem when nesting two DC sweeps (e.g., for the output characteristics of a transistor). It happens that if the inner sweep (e.g., VCE) cannot converge for one sweep point, the simulation stops without allowing the outer sweep (e.g., IB) to move to next sweep point.
Is there a solution to avoid this and to make possible the outer simulation to move to the next step without ending with error the DC analysis?
Thanks  

Outcomes