I am trying to simulate a DF-antenna system which uses a 7-port network (4 inputs and 3 outputs). The network is already built and measured with a network analyzer (using 201 measurement points). Before starting the teadious work of assembling the 2-port files from my measurement into 7-port device for simulation, what are the limitations of a s7p-file?? I am likely to have to break up the lines when setting up the matrix. Information in the manuals are not really that intuitive (i.e. for me at least::) ) I would love to see how a typical SXp net would look like with line breaks and freq notation.
Or do Eagleware support a better (smarter, simpler) way of realizing this S7p net from my two-port measurements?
/Lasse
Or do Eagleware support a better (smarter, simpler) way of realizing this S7p net from my two-port measurements?
/Lasse
There has to be a better way than you attempting to create a 7 port S-Data file. What format is your data in? I'm not sure how you turn 7-port measurements into a "bunch of 2 port files". If you have S[i,j] for i,j=1...7 which files are they found in?
Thanks,
Mark