Hi,
Is is possible to use a transistor model which was created in ADS in Genesys?
Or would you have to replicate the device along with all its parameters.
Thanks
Is is possible to use a transistor model which was created in ADS in Genesys?
Or would you have to replicate the device along with all its parameters.
Thanks
Any ADS model, having MINT interface may be loaded & used in Genesys.
Any other custom developed model may be ported in Genesys using SPICE import (if Genesys has corresponding base model implemented), or VerilogA interface.
Regards,