AnsweredAssumed Answered

whatif : dual conversionsingle frequency

Question asked by mlabro on Dec 12, 2006
Latest reply on Dec 14, 2006 by mlabro
I have just purchased whatif. It is quite nice.
I have two questions :
- can we set the bandwidth to 0MHz to simulate single frequencies (RF,OL) ?
- I have seen that we can use up to 5 mixers BUT if, I understand they must be paralleled as it is the case for multibands systems (gsm,...).
I never have such application. I always must deal with dual (or triple) conversions with two (or three) mixers in cascade. Is it possible to simulate such chain with whatif which should be very helpful to choose the OL ? If no, do you intend to develop such feature in future releases of whatif ?

Best regards  

Outcomes