Hey, fellows--
I inserted a *.JPG picture into the "notes" section of a Genesys project. (This is potentially a really cool feature, btw.)
When I emailed the *.wsp to a colleage, the picture didn't show up.
How should I go about attaching/appending the *.jpg so that it opens automatically for others?
MWI
I inserted a *.JPG picture into the "notes" section of a Genesys project. (This is potentially a really cool feature, btw.)
When I emailed the *.wsp to a colleage, the picture didn't show up.
How should I go about attaching/appending the *.jpg so that it opens automatically for others?
MWI
We hope to let you insert images into the workspace, but for now when you insert an image into notes you are inserting a URL (or path) to the image.
When you insert the file it inserts the entire file name. The only way images work consistently is to use an absolute path (full filename) which can make it tough to give to someone else (unless you have a spare webserver around, in which case you can use the web address).
If you're sharing with people on your local network this works great. Put the file on the network and use the absolute file path and everyone on your local net will see the same thing you do.
Also, notes don't always remember changes from this kind of thing, so type a space/backspace after editing images so the notes window knows to save.
Mark