is there a way for a user to "check out" a network license for a predetermined amount of time? The functionality does exist with Flexlm but I can't see this availability within the Genesys software.
On long simulations (24+ hours to run), if we have an unscheduled network outage, the simulation has to be restarted. Whereas if the license can be checked out to the workstation for a predetermined amount of time (72 hours say), the simulation will have time to complete whether the network is running or not. We are currently working on "stabilizing" the network but until this happens, something like this would really be nice.
Rob