AnsweredAssumed Answered

How to view SPICE model parameters in the GENESYS libraries

Question asked by Todd Cutler Employee on Jun 18, 2003
The SPICE model parameters in GENESYS are all available for you to view (with the exception of LDMOS which are Motorola proprietary).  The best way to see them is to open the workspace that contains the model link.  Go to the directory where GENESYS is loaded, then look in the "Model" subdirectory for the workspaces that contain each manufacturer's models.  Open the appropriate workspace and find the model that corresponds to the device of interest.  Then open the model and browse to see the model contents.  (The actual model files are SPICE netlists, directly from the manufacturer.  They are stored in subdirectories within the "Model" directory and can be viewed with any text editor such as notepad).  

Outcomes