I have a question on the following paragraph about Generalized S-parameters from the EMPOWER manual:
" In this case, you know that your port lines should be 50 ohms but EMPOWER reported 47 ohms. If you then request Generalized S-parameter, GENESYS will also use 47 ohms for the terminating impedance, and a large part of the analysis error due to the grid will be cancelled. "
Suppose EMPOWER is used to characterize a component (e.g. microstrip T-junction) and then that component is used in circuit. I understand that GENESYS uses Y-parameters for circuit analysis. Hence the S-parameters generated by EMPOWER for the component will simply be converted to Y-parameters and the normalization factor (47 or 50 ohms in above example) will have been forgotten.
QUESTION: Do Generalized S-parameters (ie. whether we choose 47 ohms or 50 ohms in above example) have any effect on the Y-parameters associated with the EMPOWER analysis?
" In this case, you know that your port lines should be 50 ohms but EMPOWER reported 47 ohms. If you then request Generalized S-parameter, GENESYS will also use 47 ohms for the terminating impedance, and a large part of the analysis error due to the grid will be cancelled. "
Suppose EMPOWER is used to characterize a component (e.g. microstrip T-junction) and then that component is used in circuit. I understand that GENESYS uses Y-parameters for circuit analysis. Hence the S-parameters generated by EMPOWER for the component will simply be converted to Y-parameters and the normalization factor (47 or 50 ohms in above example) will have been forgotten.
QUESTION: Do Generalized S-parameters (ie. whether we choose 47 ohms or 50 ohms in above example) have any effect on the Y-parameters associated with the EMPOWER analysis?
As far as I know the impedances will be irrelevant. We switched to using Y parameters with 2005, so GENESYS 2004 may have port impedance dependencies, but 2005/2006 won't, I think.
The dataset part (NPOD) specifies Y parameters as input.
Regards,
Mark