AnsweredAssumed Answered

Modifying either linear analysis or datasets

Question asked by ABOMPA on May 25, 2006
Latest reply on May 25, 2006 by MZachmann
The big change in 2006 from 2004 is the implementation of the dataset which I find very useful.  In 2006 a linear analysis is linked to a certain dataset which is somewhat inefficient since you need to  open up an analysis for each data set.  My question is this, is it possible to allow the dataset to select which analysis it uses? This would improve the efficiency since it will reduce the number of analysis which are open.  

Outcomes