AnsweredAssumed Answered

Ouput is not updated

Question asked by greite on Apr 9, 2003
:o 
I am using a post-processed expression off a linear measurement from schematic #1 in a SPA block in schematics #2. A measurement from schamatic #2 is then entered in an output window.

When schematic #1 is altered, the output related to schematic #2 is not updated. To force the update I need to open the properties dialog of the linear simulator.

Any advise ?  

Outcomes