can anyone help me with designing a mixer [down converter] for 930 MHz in Genesys. i would also like to know how to use genesys. i am pretty new to the sofware.
Genesys, while relatively easy-to-use, is a complex product. I suggest reading the Getting Started documentation and then going through the basic tutorials, followed by the ones on your particular area(s) of interest. I'll ask someone to help, regarding your mixer question.
Neal suggestions of using the Getting Started documentaion and tutorials are good. Also, there is a mixer synthesis module that sets up the entire GENESYS environment and designs 11 different mixers using diode, bipolar and FET devices.
Just start GENESYS, select New under the File menu, Right click Designs and select Add, Synthesis, Add Mixer. Give the design a name or accept Mix1. In the Mixer Type pick list, pick a mixer type. If you are just exploring, perhaps you could start with Diode Sinle Ended Basic. Click the Apply button.
You will see a schematic and output windows with spectrums at the IF and Output ports. All of this takes just a minute. Feel free to click on other graphs in the Workspace tree to open them up. Poke around in GENESYS to explore and change settings. Don't worry, if you break the setup, you can quickly repeat the above steps.
If you have specific questions, return to the forum.
Just start GENESYS, select New under the File menu, Right click Designs and select Add, Synthesis, Add Mixer. Give the design a name or accept Mix1. In the Mixer Type pick list, pick a mixer type. If you are just exploring, perhaps you could start with Diode Sinle Ended Basic. Click the Apply button.
You will see a schematic and output windows with spectrums at the IF and Output ports. All of this takes just a minute. Feel free to click on other graphs in the Workspace tree to open them up. Poke around in GENESYS to explore and change settings. Don't worry, if you break the setup, you can quickly repeat the above steps.
If you have specific questions, return to the forum.
Good luck.