I have some older .wsp files from 2004. I tried opening them with genesys 2010.05. They kindof open up, and I can view the schematic, but its format looks off. When I click on an element, like a transmission line in the schematic, all the values are empty. And, of course, the analysis will not run--errors.
If I type in values into the schematic elements, like "44" the screen shows " 44' "
I tried all the various file open options, and did not see anytning on the import tab that would help.
How come I can not open up these older files anymore? Is there a translator needed?
Rich
If I type in values into the schematic elements, like "44" the screen shows " 44' "
I tried all the various file open options, and did not see anytning on the import tab that would help.
How come I can not open up these older files anymore? Is there a translator needed?
Rich
(Man! you posted this in January, and nobody has gotten back to you from agilent? Ouch!)
Yeah, Genesys sort of went through some fundamental changes back then, and some of us (not me, necessarily) are pretty reminiscent over the good old days.
I tried following the recommended file translation procedure provided by Eagleware, but it was really painful. The easiest way +_for me_+ has been to keep a copy of 2004 on my computer and open the old and new versions in side-by-side windows. then I just create a new file using the old one as a reference. You used to be able to download and install old versions of Genesys using your current license; i don't know if that's still possible or not.
Hope that helps, if only just a little.
Mark W. Ingalls