The auto recalculation function seems do not work for EM (EM POWER &MOMENTUM GX, when change the design or simulation controller, the icon does not turn red, and need to manually click calculate button. is it the intended setting ?
It works, after simulator controller parameter changes. It does not activated by layout changes, because old Layout code does not support object notification methods, implemented in Genesys, starting from Genesys 2005.11. This is well known old Layout issue, which will be fixed in new Layout product.
It does not activated by layout changes, because old Layout code does not support object notification methods, implemented in Genesys, starting from Genesys 2005.11. This is well known old Layout issue, which will be fixed in new Layout product.