AnsweredAssumed Answered

Value in system.SerialNumber is shifted

Question asked by OnlyOne on Mar 11, 2009
Latest reply on Mar 17, 2009 by OnlyOne
Hello,
i created a testplan (TxSL6.1.1) that has also one step that writes a number into system.serialnumber via the action EchoString.umd
When i look in the report-window then i see in the header also the serial-number.

When i start TestExec and run the testplan the first time and set the serialnumber to "789" then the report looks like this:
As you can see there is no value for serial-number.
Image


When i change serialnumber to "456" and run the testplan again then the report looks like this:
Now i have the serialnumber from the first execution.
Image


When i now start the testplan again i see the serial from the second execution.

All serial-numbers are shifted by one position.
Is this the normal behaviour?

Thanks for help  

Outcomes