As of 6 May, the latest released software for the i1000 is v2.2.0p. This version brings in the BOM, PINs and Nails file into the i1000 software which helps the user to easily check for part information during debug. Also this version enhanced the "Find Pins" function. With this new enhancement, "Find Pins" now reports the selected pins almost instantly
Current released version of the i1000 software is v2.2.0p. Enhancements are ongoing to add in the new innovations like CoverExtend, etc into the i1000. So.. it's getting better each day...: )
Guess what? We just added in another feature to log all test measurements of the board in CSV format.... just load them into Excel and you can have your CPK, STDEV, etc report in a matter of minutes !