Hi we have some difficulties programming Atmega32. We also program atmega8 and 16 without any issues. With a read action for example (blank check), the maximum number of words which can be read at once is 256. To read the full flash, I need 64 VCL tests. This increadible and not necessary. I think that the device is out of synchronisation and out of ISP mode. Can someone provide me a working lib ( maybe we can trade, we program many different types of processors).
A long time ago I make the program for ATMega, see attached files. If you need more help about this tell me - ok?
Luiz Silva
Development In-circuit test engineer.