AnsweredAssumed Answered

High Current Power Supply

Question asked by yenuplaotis on Feb 28, 2012
Latest reply on Feb 28, 2012 by adrianc
Are there any high current (>2A) high voltage (~50V) DUT Power supplies available for powering large boards with 48V Bricks available?  How does one set one up as a Standard 3070 supply?  I know that you can put 6624A outputs in parallel but this becomes painful when the input return line on the Brick is always isolated from the Board Ground used for digital testing.  You are then stuck either providing special power supply wiring instructions to the fixture vendor or removing and re-wiring the Supply Lo and Lo Sense.  Both of these options are opportunities for error.  Any suggestions are very much appreciated.  

Outcomes