Hello everyone, I have a hopefully quick question. We are trying to find a way to use some i5000 files (unmuxed hybrid double density 144 cards) on either a hp3070 unix system version 5.21 or an i3070 version 7.2 (hybrid standard double density cards). All we really want to be able to do is to verify the probe, transfer, and testjet wiring without having to individually ohm out each connection manually with an ohm-meter and the wirelist (or creating a dummy config file and using the find pins function). Getting working pins and shorts tests would be nice too. Will this be possible or do we just need to create a dummy config file and use find pins for the hybrid card connections and an ohm meter for the control card, asru, and tesjet connections?
if you develop using 7.2 there should be an option in IPG to make 'transportable' the fixture. I have shown the options below - this means you can debug an unmux fixture on a mux system - is this what you were looking for?
if you dont do this at development then you are too late this time, the main difference is on analog structure, so you 'might' be able to workaround but its not so pretty
Select whether you want to generate a transportable fixture:
Mux-specific Fixture – for Mux system only
Mux/UnMux Fixture – transportable between UnMux and Mux systems