I am trying to use the autofile for an setup that includes an adapter. I have made a custom operator keypad in the .hp3070 file and just need to finish making a button that uses the autofile to switch directories and load the board. I can not find where the code is that executes when "fixture lock" and the "run testplan" buttons are pressed on the initial operator keypad.
I am using and adapter that locks to the testhead when the "fixture lock" is enabled for fixtures that were not developed for the 3070. Then the actual board fixture is placed on the adapter. I then issue a fbon to lock the fixture to the adapter. Now I am able to read the autofile.
I am using and adapter that locks to the testhead when the "fixture lock" is enabled for fixtures that were not developed for the 3070. Then the actual board fixture is placed on the adapter. I then issue a fbon to lock the fixture to the adapter. Now I am able to read the autofile.
It is under /Agilent/lib/sys.Operator