I need to take repetitive runs and then stop and look at a run which displays an error.
I do not want to look back through many, many old saved repetitive runs before finding the one which contained the error.
What should I do?
I do not want to look back through many, many old saved repetitive runs before finding the one which contained the error.
What should I do?
Start the agLogic main application GUI -> load your configuration -> craft a trigger spec which causes repeatability -> Run to take the first trace -> this is now your 'good' trace -> Window -> New Compare -> raise the Compare Window -> Copy... -> MyBus1 (or whatever) -> Add -> OK -> you will now see a 'reference' column in your Compare Window -> Run/Stop -> Run Properties... -> check Save after ever acquisition but do NOT check Increment file number between runs -> browse to a known path and base file name for saving runs -> Note that it will now use the base file name over and over and over again , also do NOT check stop after n runs -> OK -> raise the Compare Window -> Run Until... -> enter the number of differences allowed between a current trace and your golden reference trace , presumably 1 , and check Stop Repetitive Run -> Apply -> OK -> Now cliock Run/Stop -> Run Repetitively
And, it will stop the very first time that it takes a trace which did not compare properly with your golden reference trace and it will leave that last trace in your base file name and path.
It will not create vast numbers of traces in the path.
Rather there will be only one and it will be that one which had a difference from your reference trace.