The 16720A has a Run Repetitive button in the user interface. It is important to remember that Initialization code runs once at the beginning of the run. The code in the body of vectors runs repetitively. There is no fill added to the vectors. This feature allows the equivalent of an infinite loop.