AnsweredAssumed Answered

Limit-names in report

Question asked by OnlyOne on Dec 2, 2008
Latest reply on Dec 3, 2008 by jinho
Hello,
when i create a test with some identical actions inside (for example echoInt32), then i can create a limit for each action. In the Limit-tab the limits are then numbered with:
"EchoInt32 #1 (Result)"

But when then testplan executes and i look in the report then it only displays:
"Limit EchoInt32 Result FAILED"

But its not clear which of the EchoInt32-action is failed.

Is it possible for future releases to add in the report also this "#1"?
Then someone could reconstruct where to look in the testplan.
If i only report fails then noone ever knows where to look.

best regards  

Outcomes