AnsweredAssumed Answered

EMF MEasurment

Question asked by rnarasingarao on Dec 6, 2010
Latest reply on Dec 7, 2010 by xingsali
Will the Model:N9342C is suitable for the below Measurments if yes what are the options are to be taken along with the standard. And to measure i need to Use ISOTROPIC antenna also please do let me know the availability of ISOTROPIC antenna with freq range from 30 MHz to 3GHz.

I need to measure the E-field, H-Field & power density in air.
E-field V/m
H-Field A/m
Power density Min W/m^2.  

Outcomes