AnsweredAssumed Answered

Screen & Data Grab for FieldFox

Question asked by chrisjardine on Jul 28, 2010
Latest reply on Jul 28, 2010 by am95405

Hi,

 

I'm trying to automate the collection of data using a N9912A connected via a direct LAN connection.

 

I understand how to acquire the trace data (and hopefully then be able to dump that to an Excel sheet), but is there any way I can get the Fieldfox to do a screendump to a file, hopefully the same sheet used for the data, over the LAN as opposed to a USB drive or using the internal memory?

 

Secondly, I'd like to be able to define data capture to occur at user-defined times- i.e. take a plot every 5 seconds between time x and time y- is this possible?

 

Regards,

 

Chris  

Outcomes