AnsweredAssumed Answered

N9330B Frequency Range

Question asked by rjf19 on Jan 20, 2010
Latest reply on Jan 20, 2010 by rjf19
This is basically a note to Agilent. I would love to see an extension in the lower frequency range of the N9330B to 2MHz or, at least 5MHz. Some of us still work in the trenches from time to time or dabble in Ham Radio on the side and the ability to sweep antenna and feed line installations at the lower frequency bands would certainly be an option I would pay for. Right now, I need to maintain multiple analyzers to accomplish this, sure would like to lower that to one unit! 

Robert J Fehn Sr
Director of Information Technology
St. Mary’s County Metropolitan Commission
301-373-4733 Ext 218
bfehn@metcom.org
http://www.metcom.org

Outcomes