AnsweredAssumed Answered

Is there a better way to define Harmonics for Multipliers?

Question asked by jhoffm on Apr 27, 2004
I want to simulate a radar system, which uses a number of multipliers of high order (90+). How can I define the harmonics for these without typing 90+ numbers into each multiplier's Parts Properties window?
I tried to use Equations, which still isn't a great method, by

H1=-100;-90;...;0;...-90;-100

but that didn't work.

Can I use a table or do I actually need to type all of these numbers into each part?  

Outcomes