AnsweredAssumed Answered

How can we use Modelitics libraries ?

Question asked by mlabro on Feb 9, 2004
I have just purchased Modelithics library for 1008cs inductors from Coilcraft.
I have designed and optimized a filter which involves a 680nH Q=45 inductor.
Now, I'd like to replace this ideal inductor with the Coilcraft 1008cs-681XGBC present in the Modelithics library.
How can I do that ? Where are the modelithics models located in genesys workspace ? I have received no manual concerning these libraries.

Marc  

Outcomes