AnsweredAssumed Answered

controlling Optimization results

Question asked by zbar-k on Jan 11, 2004
Latest reply on Sep 17, 2004 by skelly
Hi,

  I used to be able to control the optimization process by using F5 and ****+F5. If I was not satisfied with the results of the optimizer I would simply stop it (esc) and press Shift+F5.

it seems that in the version I'm using (2003.03) I cannot do this. Stopping the optimizer automatically saves the current components values (whether I like it or not) and pressing Shift+F5 do not return the components back to the original values.

Is there a way a could revert back to revious versions operation practice?

This is an exteremely annoing issue for me.

Zvika Bar-Kochva
Mainnet Communications  

Outcomes