Say I have two designs, Sch1 and Sch2. In Layout1 both designs are included. I would like to add a "rubber-band" connecting the output of Sch1 to the input of Sch2.
This would enable one to split a complex design into smaller managable circuits and yet keep the complex layout connected together.
Danny
This would enable one to split a complex design into smaller managable circuits and yet keep the complex layout connected together.
Danny
If including Sch1 and Sch2 on a third schematic would work as expected and (at the user's option) create all elements of sch1 and sch2, would that work for you? If that worked, simulation would be easy from the combination, too.
Rob Lefebvre