How can I view S-parameter data which is embedded in workspace-file? Example: the example file of V7.52 "Amp Noise.wsp" gives the warning / info "Cannot find s-par.... Using workspace's copy instead..."
The S-Data file doesn`t incude into workspace. It just linked. So you realy have some work files: your Workspace, S-Data files ane library. So you need to keep all this files for your project work propertly. Good luck!
Actually, the workspace DOES include copies of s-parameter files automatically. Currently, however, GENESYS does not allow you to directly view these. These is an unreleased utility that we use at Eagleware to view these files and to clean out a workspace. I will see if it will be possible to post this utility here for general use.
In future versions of GENESYS, we expect to make this directly accessible within the software.
Good luck!