AnsweredAssumed Answered

N5230A - not connectic with USB

Question asked by mirek on Apr 13, 2016
Latest reply on Apr 13, 2016 by christopher_rich@keysight.com
I am trying to control PNA-L N5230A thru USB connection, but it look like the PC do not see the Network Analyzer.
I used connection Agilent IO control (16.3) to detect the PNA but it not show up on the USB list. In the same time I can connect USB-to-GPIB and I can see that Network Analyzer in the list.
Look like the USB B input is off or missing driver. I look in the control panel hardware configuration and I see that all USBs work properly.
What do I missing in there. The firmware on the PNA-L is A.7.50.67 with 1.1GHz CPU.

Any advice how to fix that?  

Outcomes