In the company we have several computers loaded with eagleware 2004.7. In one of the computer (P4 3.2 GHz, 2GB RAM, Win XP Pro OS ) the processor usage is not even reach to 5% when I make the optimization. However some other slower computers allocate full usage of the computer resources and they work much (1 : 10) faster than the previous computer. As an example, During the optimization process One computer goes on 2 round, other one goes 12 th round of the optimization process.
Is there something wrong in the software or hardware?
Is there something wrong in the software or hardware?
To confirm this, you can boot your computer into safe mode and then run GENESYS. If GENESYS speeds up, you then need to figure out what caused the conflict.
Rob Lefebvre