I am using Genesys 2004.03. I have an S parameter transistor file which covers 10 MHz to 3 GHz. When I do a linear Analysis using log sweep over this range, I get a local error indicating "... does not cover the analysis frequency range..." Further, when I reduce the frequency range so that it is definately inside this range, the error is not cleared unless I shut down and re-start the software. What can I do to clear this error without having to re-start Genesys?
Also, in version 2004.07, if you fix the range and then open the part properties box of the part that is causing the error, close it, and update the simulation, the error should clear.
[file]log range.wsp[/file]
Attachments