I use a NPO model to include S parameters files in my simulations. The file name is defined in the equation block and depend on a variable parameter (an index for example).
In 2003 version, it was possible to sweep this variable or to tune it, and the S parameter file was updated.
in 2004.07, when the filename change during sweep or tuning, the simulator does not re-read the new file and nothing change.
I found only one solution: edit the NPO properties, then the simulations are updated.
is it a solution to use sweep or tuning?
In 2003 version, it was possible to sweep this variable or to tune it, and the S parameter file was updated.
in 2004.07, when the filename change during sweep or tuning, the simulator does not re-read the new file and nothing change.
I found only one solution: edit the NPO properties, then the simulations are updated.
is it a solution to use sweep or tuning?
to as an "unintended feature". That is, it (creative use of
equations and number indexing to form a filename for automated
indexing among datafiles) worked but we weren't aware that
people applied the function in that way, and thus it wasn't specifically
maintained as a "feature". Some other changes within Genesys
apparently disabled this feature. I have made our developers
aware of this, and it is logged as service item #3002 at Eagleware.
I expect that this will probably be reintroduced as an acknowledged
feature in a future release of software, but I'm not able to provide
specific ETA.