would be great if it was possible to select multiple/all files in the "Manage cached files" window. For workspaces that I use as a template/starting point for other files, the s-parameter files tend to "pile up" and inflate the size of the *wsp file.
I tend to forget that the *.wsp file cached all the s-parameters files ever used and one workspace shrank down from 11MB down to 1MB after I deleted the old cached files.
Is the caching of s-parameter files that are no longer used in any schematic intentional? I would have thought that keeping the ones used in the schematic would be enough.
I tend to forget that the *.wsp file cached all the s-parameters files ever used and one workspace shrank down from 11MB down to 1MB after I deleted the old cached files.
Is the caching of s-parameter files that are no longer used in any schematic intentional? I would have thought that keeping the ones used in the schematic would be enough.
I'll look into a "select all" option. As for why the files "pile up" the answer is that it's almost impossible for us to tell which files are still used so we just never delete them. The way files are referenced (via FILENAME in a bunch of models and by using the name in the second page of a part property and via ... ) we just can't effectively keep track of them all.
We cache the data so that you can transfer files to other people and have them still work.
Mark