AnsweredAssumed Answered

FTP'ing into a 9020A MXA?

Question asked by raphael on Dec 15, 2008
Latest reply on Dec 15, 2008 by raphael
I am using an MXA 9020A with the 802.16 OFDMA personality and would like to import a map file that does not reside locally on the MXA.  My preferred solution would be to simply write a script to FTP the .SCP file into the MXA and then load it locally. The MXA FTP server accepts "Administrator" and "agilent4u" as valid credentials, but the permissions are not enabled to write to the home directory, nor can I 'ls' or 'cd' to any other directory.  I have searched but am unable to find any information about this so I'm not sure if what I'm trying to do is supported.   Thanks in advance.  

Outcomes