AnsweredAssumed Answered

How to automate "89600 VSA - ACP" test via COM API?

Question asked by sherry2010 on Apr 6, 2010
Latest reply on Apr 8, 2010 by tabbott
We tried to implement an automated ACP test software via 89600 VSA's COM API for my N9010A.

By Manual Test
- 1. Starting the "LaunchXSA" icon from the N9010A.
- 2. Hit "Meas" and then select the "ACP" button on the application
- 3. We then recall a pre-recorded state file (xxx.state) and then we have the following test ready for ACP test.

Image
- 4.record the bottom summary of Lower and Upper dBC and dBm

Question: How can we achiever step 2 & 3  by the COM API interface? Is it a VsaScalar or TEDS or something else? We'd like to implement an automated application to run with XSA which we can input different power/freq for different results. We are doing this manually now.  

Attachments

Outcomes