Is this true? I see there is an option for ADC2, but the help makes it sound as though this is only functional if a 2 Channel VXI analyzer is used. I'm unable to select my DSO as the source even though it shows up in the form. Once I check it, the OK button gets greyed out.
I'm running VSA version: 7.20 (build 7.20.0114)
and I have a DSO81204B 4CH
and a 54855A 4CH
...used as HW.
Is there any plans for future support of this capability?
Thanks,
Daniel
I'm running VSA version: 7.20 (build 7.20.0114)
and I have a DSO81204B 4CH
and a 54855A 4CH
...used as HW.
Is there any plans for future support of this capability?
Thanks,
Daniel
It is true that you cannot have two Scopes each selected as a different ADC for 89600 VSA. The only two channel, multiple input, option with this setup is to utilize the channels of the Scope as the individual I and Q inputs.