I have a problem to measure the Baseband noise on E5052A SSA. I see the function in E5052B, but not in E5052A. I did load the new FW 2.51, but it does not have Baseband measurement in the main measurement menu. The E5052A do have input for the Baseband. Can it be use and how?
The BNC connector on the E5052A is not functional - there is no way to measure baseband noise.
The hardware was changed, and the baseband noise input function is available on the E5052B - but not on the E5052A. Sorry!