With option 011, the perpetual node locked license, the FPGA dynamic probe is licensed to the logic analyzer (1680 Series, 1690 Series, 16800 Series or 16900 Series). Multiple instances of the FPGA dynamic probe are provided so you can use a single license for all logic analysis modules in the system.
With option 012, the perpetual floating license, you have one instance of the FPGA dynamic probe that can be used by any 1680 Series, 1690 Series, 16800 Series or 16900 Series logic analyzer that has access to the license server.
the FPGA dynamic probe is licensed to the logic
analyzer (1680 Series, 1690 Series, 16800 Series or
16900 Series). Multiple instances of the FPGA
dynamic probe are provided so you can use a single
license for all logic analysis modules in the system.
With option 012, the perpetual floating license, you
have one instance of the FPGA dynamic probe that
can be used by any 1680 Series, 1690 Series, 16800
Series or 16900 Series logic analyzer that has access
to the license server.