I have a 16700B analyzer - can it support the Iomega ZIP drive (SCSI)?
Problem I have is that only SCSI ID 3 or 4 are offered in the 16702B LA menu, but the Iomega only can select SCSI ID 5 or 6 (rear panel switch).
In the manual, the SCSI Hard drive has ID 6 and the CDROM has ID 1. So SCSI ID 5 is unused.
Why can't I select SCSI ID 5 in the menu for the logic analyzer?
Or is there a way to "hack" the Iomega drive to support SCSI ID 3 or 4?
Regards,
Mike
Problem I have is that only SCSI ID 3 or 4 are offered in the 16702B LA menu, but the Iomega only can select SCSI ID 5 or 6 (rear panel switch).
In the manual, the SCSI Hard drive has ID 6 and the CDROM has ID 1. So SCSI ID 5 is unused.
Why can't I select SCSI ID 5 in the menu for the logic analyzer?
Or is there a way to "hack" the Iomega drive to support SCSI ID 3 or 4?
Regards,
Mike
I would say that the probability of getting this to work is very low.
Al